Let's Connect!
Sign up to receive exclusive communications about offerings, events, news, surveys, special offers, and related topics via telephone, email and other forms of electronic communications.
HYDRANAL™ Laboratory Report L 288
For water determination in nitrogen bases, the existing literature states:
In general, these statements are correct. However, they appear rather vague and therefore we tried to make more precise statements and develop more exact titration methods.
We examined over 100 separate amines using the 3 common titration techniques:
We followed this basic procedure for each technique:
Parameters measured were the following:
The titration medium was acidified by:
The following reagent combinations were tested:
1. Volumetric one-component technique
Hydranal-Composite 5, in combination with the following working media:
2. Volumetric two-component technique
Hydranal-Titrant 5, in combination with the following working media:
3. Coulometric determination
5 mL Hydranal-Coulomat CG as catholyte, in combination with the following anolyte solutions:
The titrations curves were evaluated, the results can be found in the table at the end of this report.
1. Aliphatic amines
Aliphatic amines are strongly basic and must be titrated in the presence of benzoic acid. According to the literature, the amount of sample added is limited in order to ensure that the neutralizing capacity of the added acid is not exceeded.
n-Propylamine
When testing the recommendations with n-propylamine, the statement seems to be confirmed. After more exact investigation it shows that the recovery of 5 mg added water is slightly too high (about 102%). With setting more stringent end-point conditions and an end-point drift of 10 μL/min, an end-point is no longer obtained with this standard determination. Hence it must be concluded, that a slight side reaction occurs during the analysis of n-propylamine.
Coulometric determination in the presence of benzoic acid (5 x 0.5 g of n-propylamine) shows a drift increase after each sample addition. It must therefore be concluded that the same side reaction occurs with n-propylamine.
2-Aminoethanol
When titrating 2-aminoethanol volumetrically, no end-point is found with addition of benzoic acid. Only with the addition of salicylic acid a 2 g sample can be titrated as usual. Therefore, salicylic acid is recommended rather than benzoic acid.
The same is valid basically for the coulometric determination. The titration of small samples in the presence of benzoic acid results in a small increasing drift and a slightly higher recovery rate of water.
This increasing drift generally affects the limitations of coulometry in different ways:
The addition of salicylic acid would also improve the titrations characteristics for coulometry. The drift increase is smaller and thus the amount of sample, which can be titrated, is larger. However, there is another much higher risk in this case.
Salicylic acid is oxidized by the anode under certain conditions and, therefore, poisons the electrode of the coulometer. This always takes place if the salicylic acid is to a large extent neutralized and the pH rises above 5 again. Because of this we do not recommend the use of salicylic acid for coulometry.
For aliphatic amines our investigation resulted in a few different titration methods, which are listed in table at the end.
Most amines were titrated with the addition of benzoic acid. For the two-component reagents, salicylic acid is preferred in some cases. For coulometry, small samples are applied to avoid a too high drift increase between samples. Secondary and tertiary amines behave clearly different. They cause by far less problems than primary amines. That means that for coulometry also the amount of sample used depends only on the neutralizing capacity of the benzoic acid.
2. Aliphatic Diamines
The titration of 1 mL 1,2-diaminoethane (ethylenediamine) as a free base and in the presence of benzoic acid or salicylic acid, shows much more problems than with monoamines. Also, the difference between benzoic acid and salicylic acid is greater. Even salicylic acid suppresses the side reaction insufficiently, so that only relatively small sample weights can be titrated in this group of compounds.
Table at the end shows examples of diamines that were investigated.
With the two-component reagents it is only possible to titrate small quantities of sample, only with the strongly acidic sulfite buffer. Actually, these titrations should be classified as non-recommendable. Coulometry is generally not possible for this group of compounds, with the exception of hexamethylene diamine, which can perhaps be accepted as a compromise for water determination.
3. Cyclic Amines
Table at the end shows some examples for cyclic amines. They behave like secondary amines except for a less pronounced side reaction and a slightly lower basicity. In this case, the addition of benzoic acid is sufficient. For coulometry the addition of benzoic acid is not required. The neutralization capacity of the reagent is sufficient because the quantity of amine added is clearly limited by the increasing drift.
4. Aromatic Amines
Aromatic amines only react as weak bases. It should therefore theoretically be possible to titrate them without problems. In practice there are clearly different findings. The titration of 5 g aniline in methanol gives no end-point, due to a very strong side reaction. Addition of benzoic or salicylic acid reduces this side reaction, although still no end-point is found. Reducing the sample weight to 2 g leads to an end-point in the presence of salicylic acid, although it also depends on the instrument settings because the side reaction is only reduced, but not prevented.
This different behavior clearly contradicts our expectations. Obviously the side reaction is much more pronounced and not completely suppressed by addition of acid. From earlier investigations we know that aniline is methylated in the KF medium, therefore it can produce N-methylaniline. This side reaction could be the cause for the problematic titration. We replaced the methanol by 2-chloroethanol and carried out the determination in Hydranal-Working Medium K. The side reaction was clearly weaker, and in the presence of salicylic acid a sufficiently stable end-point can be obtained.
Since Hydranal-Working Medium K was declared as very toxic, in 2009 we made further investigations and found Hydranal-Buffer Base perfectly suited, as methanol is widely replaced by ethanol. 5 mL of aniline can be determined with a very stable end-point.
Amongst certain substance groups, the differences are very large. For substances that are easily oxidized like 2-aminophenol, the sulfite buffer is preferred because it is more acidic than salicylic acid and the side reaction is even further suppressed. Using the two- component reagents, the addition of sulfite buffer is strongly recommended.
N-substituted aniline derivatives are less sensitive to the side reaction and may be analyzed using the volumetric standard procedure. All phenylene diamines are very sensitive to this reaction and have limited applicability even with the one-component reagents.
With coulometry all aromatic amines are very easily oxidized (or methylated), so methanolic reagents are generally not suitable. Even in the strongly acidic sulfite buffer, only small quantities can be analyzed and the recovery rates are also still too high. Only the methanol-free reagents Hydranal-Coulomat AK and Hydranal-Coulomat CG-K are suitable for this group of substances, additionally the sample size is limited to only 2 g. Also with coulometry the differences in chemical structure become noticeable. N-substituted aniline derivatives can be added in larger quantities, just as diphenylamine. Coating of the anode should not be overlooked, this often occurs sporadically with different aromatic amines. Also, recovery rates are observed to be too high, thus control of the recovery rate with Hydranal-Water Standard is strongly recommended.
5. Heterocyles
Heterocyles are weakly basic and chemically very similar, so most of them can be titrated according to the standard procedure (see table at the end).
But there are also exceptions. For benzimidazole or 1,2,4-triazole the sample weight is limited, since the substance has only limited solubility. For 2-aminopyridine or 2-aminobenzothiazole it is necessary to add benzoic acid for the volumetric titration in order to sufficiently suppress this side reaction.
Greater difficulties appear with coulometric determination in this group of compounds. For some condensed heterocycles it is advisable to add sulfite buffer, for others coulometry is generally less recommended.
Summary and Chemical Reasoning
After evaluation of all these results, the following conclusions can be made:
Legends for the Table
Me: | 30 mL Hydranal-Methanol dry | |
So: | 30 mL Hydranal-Solvent | |
AG: | 100 mL Hydranal-Coulomat AG | |
Me + Be: | 30 mL Hydranal-Methanol dry | + 5 g benzoic acid or 30 mL Hydranal-Buffer for Bases |
Me + Sa: | 30 mL Hydranal-Methanol dry | + 5 g salicylic acid or 30 mL Hydranal-Buffer for Bases |
Me + Bu: | 20 mL Hydranal-Methanol dry | + 15 mL sulfite buffer |
Wm + Sa: | 30 mL Hydranal-Working Medium K | + 5 g salicylic acid |
So + Be: | 30 mL Hydranal-Solvent | + 5 g benzoic acid |
So + Sa: | 30 mL Hydranal-Solvent | + 5 g salicylic acid |
So + Bu: | 15 mL Hydranal-Solvent | +15 mL sulfite buffer |
A + Be: | 100 mL Hydranal-Coulomat AG | +20 g benzoic acid |
A + Bu: | 100 mL Hydranal-Coulomat AG | +20 mL sulfite buffer |
AK | 100 mL Hydranal-Coulomat AK | |
L: | Added as a solution in methanol | |
(L): | Solubility on addition of the sample | |
T: | Clouding on addition of the sample | |
N: | Precipitation on addition of the sample | |
... g: | Sample amount |
HYDRANAL- Composite |
HYDRANAL- Solvent / Titrant |
HYDRANAL- Coulomat |
|
Aliphatic ketones n-Propylamine iso-Propylamine n-Butylamine 1-Hexylamine 3-Methoxypropylamine Tris-(hydroxymethyl)-aminomethane 2-Aminoethanol Cyclohexylamine Dipentylamine Dicyclohexylamine Diethanolamine Triethylamine N,N-Dimethylethanolamine Triethanolamine N,N-Dimethylcyclohexylamine |
Me + Be 1.5 g Me + Be 2 g Me + Be 2 g Me + Be 3 g Me + Sa 3 g Me + Be 3 g Me + Sa 2 g Me + Be 2 g Me + Be 3 g Me + Be 3 g Me + Be 5 g Me + Be 4 g Me + Be 3 g Me + Be 5 g Me + Be 4 g |
So + Sa 1 g So + Sa 1.5 g So + Sa 1.5 g So + Sa 3 g So + Sa 2 g So + Bu 3 g So + Bu 2 g So + Be 2 g So + Be 4 g So + Be 2 g So + Be 4 g So + Be 4 g So + Be 2 g So + Be 5 g So + Be 4 g |
AG + Be 10 x 0.2 g AG + Be 15 x 0.2 g AG + Be 10 x 0.2 g AG + Be 15 x 0.2 g AG + Be 15 x 0.2 g AG + Be 20 x 0.1 g AG + Be 10 x 0.1 g AG + Be 25 x 0.2 g AG + Be 20 x 0.3 g AG + Be 15 x 1 g AG + Be 15 x 0.5 g AG + Be 15 x 0.5 g AG + Be 15 x 0.5 g AG + Be 15 x 0.5 g AG + Be 20 x 0.5 g |
Diamines 1,2-Diaminoethane (Ethylenediamine) Appl. L 027 Diethylenetriamine Appl. L 026 Triethylenetetramine Appl. L 026 Tetraethylenepentamine Appl. L 026 3-(N,N-Dimethylamino)-Propylamine Hexamethylenediamine |
Me + Sa 0.5 g Me + Sa 1 g Me + Sa 0.5 g Me + Sa 0.5 g Me + Sa 1.5 g Me + Sa 2 g |
So + Bu 0.5 g So + Bu 0.5 g So + Bu 0.5 g So + Bu 0.5 g So + Bu 1 g So + Bu 0.5 g |
not measurable not measurable not measurable not measurable not measurable AG + Bu 20 x 0.2 g |
Cyclic Amines Pyrrolidine Piperidine 1-Methylpiperidine Piperazine Morpholine |
Me + Sa 1 g Me + Be 3 g Me + Be 3 g Me + Be 1.5 g N Me + Be 3 g |
So + Be So + Be So + Be So + Be 1.5 g N So + Be 3 g |
AG 10 x 0.1 g AG 20 x 0.2 g AG 20 x 0.5 g AG 10 x 0.2 g AG 20 x 0.5 g |
Aromatic Amines Aniline Appl. L 030 o-Toluidine m-Toluidine 4-Anisidine 2-Aminophenol 1-Naphtylamine N-Methylaniline N,N-Dimethylaniline N,N-Diethylaniline Diphenylamine 1,2-Phenylenediamine 1,3-Phenylenediamine 4-Methyl-1,2-phenylenediamine |
Wm + Sa 5 g Wm + Sa 5 g Wm + Sa 5 g Wm + Sa 3 g Me + Pu 2 g Wm + Sa 5 g Me 5 g Me 5 g Me 5 g Me 5 g Wm + Sa 1 g Wm + Sa 1 g not measurable |
So + Bu 1 g So + Bu 1 g So + Bu 1 g So + Bu 1 g So + Bu 1 g So + Bu 2 g So 5 g So 5 g So 5 g So 5 g not measurable not measurable not measurable |
AK 15 x 0.1 g AK 10 x 0.2 g AK 10 x 0.1 g AK 10 x 0.1 g L not measurable AK 20 x 0.2 g L AK 20 x 0.5 g AK 20 x 0.5 g AK 40 x 0.5 g AK 10 x 0.5 g L not measurable not measurable not measurable |
Heterocycles Pyridine 1-Picoline Quinoline Imidazole 1-Methylimidazole Benzimidazole 1,3,5-Triazine 1,2,4-Triazole Benzothiazole Pyrrole Indole Carbazole Nicotine 8-Hydroxyquinoline 2-Aminopyridine 3-Aminopyridine 2-Aminobenzothiazole |
Me 5 g Me 5 g Me 5 g Me 5 g Me 5 g Me 1 g Me 5 g Me 1 g Me 5 g Me 5 g Me 5 g Me 0.2 g (L) Me 4 g Me 5 g Me 5 g Me + Sa 3 g Me + Sa 5 g |
So 5 g So 5 g So 5 g So 5 g So 5 g So 1 g So 5 g So 1 g So 5 g So 5 g So 5 g So 1 g (L) So 3 g So 5 g So 5 g So + Sa 2 g So + Sa 2 g |
AG 20 x 1 g AG 20 x 1 g AG 20 x 1 g AG 20 x 1 g L AG 25 x 1 g L AG 10 x 1 g L AG 12 x 0.5 g L AG 10 x 0.5 g L AG 40 x 0.5 g AG + Bu 30 x 0.2 g not recommendable AG 10 x 0.05 g (L) AG 10 x 0.2 g AG + Bu 10 x 0.5 g L AG + Bu 15 x 0.5 g L not recommendable not recommendable |